Time is precious these days so the less time (and space) you need to charge all of your gadgets the more time you have for… everything else!
Every device we own requires a two or three-part charger. The phone charger connects to a large adapter, which then plugs into a duplex outlet, subsequently blocking the lower outlet and making it useless. Before I can even find the nearest empty outlet, the tablet is dead. To make matters worse, all these wires and bulky adapters tangle up constantly - when they can actually be found!
Well, those days are over! Awarded a 2013 NECA Showstopper (National Electrical Contractors Association), The new Leviton 4-Port USB Charger Device is designed for one reason - to simultaneously charge 4 high-powered devices so you spend less time charging and more time enjoying your devices. Each port is vertically positioned, making wire clutter a thing of the past, and the device itself is equipped with a microprocessor and smart chip that recognizes the charging power of each device for maximum charging in minimal time.
Functionality is now fully acquainted with style, and the friendship couldn’t be more timely. Cell phones have replaced landlines, tablets are replacing computers, eReaders are replacing books and for these devices (and many others) the USB has replaced the plug! Leave it to Leviton to pioneer the future of electronics, always with finesse, and never without genius.