Like many industries, construction is facing challenges related to filling the ranks in its workforce. Hispanic construction workers are the primary demographic seen filling those gaps in the industry. Recent statistics from The Bureau of Labor Statistics show that over 90% of the construction industry, as a whole, are males and more than 88% are Caucasian. However, 46.7% of laborers are Hispanic and it’s estimated that over 75% of the construction workforce is Spanish speaking. With the 2021 US Census Bureau showing that the United States is continuing to diversify, it’s important that the industry considers evolutions to the workforce and how to ensure representation and inclusion of multicultural talent in everyday jobs.
Why Now?
With the nation’s ambitious climate and sustainability goals, construction workers are in high demand to advance clean energy infrastructure and electrification. Renewable and clean energy systems such as electric vehicles, electric vehicle charging stations, solar panels, heat pumps and more require specialized skills, knowledge and support from electricians and other skilled construction workers. According to a recent report from Rewiring America, one million additional electricians are needed in the United States to make these important infrastructure updates. The US Bureau of Labor Statistics also projects a 9.1% growth in electrician jobs from 2020 to 2030. Electricians are needed now more than ever, and retaining diverse talent in the industry can help minimize labor shortages and advance electrification.
Recognize, Embrace and Seek-out the Solution
Consider the following to attract and retain a more diverse construction workforce:
The Bottom Line
The clean energy movement is quickly escalating, and there is already a shortage of electricians in the US. Attracting and retaining diverse talent in the construction industry can help. There is a tremendous opportunity for new talent to pursue a career in construction.