Leviton GFCI Circuit Breakers Deliver Safety Ahead of Their Time

Leviton GFCI Circuit Breakers Deliver Safety Ahead of Their Time

Like you, we take safety seriously. As the market leader in ground-fault protection, Leviton naturally engineered the GFCI and Dual Function AFCI/GFCI circuit breakers in our new Leviton Load Center using state-of-the-art technologies that provide added layers of safety over traditional residential circuit breakers. 

But what does this really mean? Simply put, unlike others, Leviton circuit breakers with GFCI technology offer more complete End of Life protection. And that means everything when helping to ensure the safety of homeowners and their families.

GFCI End of Life

GFCI End of Life is defined by UL as when a GFCI is incapable of providing ground-fault protection and passing its internal test function. Unlike competitors, Leviton circuit breakers with GFCI technology deny the user the ability to reset once the GFCI reaches end of life. By cutting the flow of power, which is now unprotected, they provide the most complete protection against electrical shock.

To meet the requirements of the UL Standard, seven critical components of the GFCI are tested. But did you know that until very recently, circuit breakers with GFCI technology were exempt if two of the seven components failed?

These exceptions for the two components make it possible to reset and turn ON certain GFCI circuit breakers, allowing them to continue to provide unprotected power without alerting the end user.

This gap in protection, and in homeowner safety, is why Leviton designed our circuit breakers with GFCI technology to deny power if any of the seven components failed. This provides more complete protection – no exceptions.

But that’s not all. Leviton successfully submitted a proposal to UL requesting their Standard be updated to mandate that ALL circuit breakers with GFCI technology meet the same End of Life safety requirements. But even though the UL Standard has been revised, manufacturers are still given over three years to improve their design to conform.

Three years is a long time. Why settle when you can have more complete End of Life protection now?

Leviton. The brand you trust for the protection you need.

For more info, visit Leviton.com/eol

 


LEVITON CIRCUIT BREAKERS

LEVITON CIRCUIT BREAKERS WITH GFCI TECHNOLOGY ARE THE ONLY CIRCUIT BREAKERS ON THE MARKET THAT ARE ALREADY COMPLIANT TO THE NEW UL STANDARD. Learn more at Leviton.com/LoadCenter