With lower transceiver costs, superior longevity, distance and upgradeability, OS2 fiber is an increasingly attractive option for data center and...
The phrase "a cluttered desk is a sign of genius" does not extend to network cabinets.
Small-diameter 28-gauge copper patch cords can offer big advantages in commercial networks, helping alleviate congestion and improve airflow in high-...
Below are some highlights of active projects from committee meetings during the third quarter of 2019.
Polarity is a critical part of any fiber network. In a nutshell, polarity means that a fiber optic link’s transmit signal at one end of the cable...
Read highlights of active projects from committee meetings during the third quarter of 2019. These include developments in standards for single-pair...
Industry standards are an important tool for data center design. The standards created by ISO, IEEE, and TIA ensure the interoperability of equipment...
Due to new transceivers, coupled with customer needs and network requirements, the market is ignoring the new, unproven OM5 cable and sticking with...
The design and deployment of data centers is as much an art as it is a science.
IEEE 802.3 meeting, the Next-Gen Multimode 200 and 400 Gb/s study group voted down physical layer specification that supports 200 Gb/s operation over...